我有一路50M的时钟信号需要转成16路同步的LVDS差分时钟信号走背板给FPGA芯片,我看了一下SN65MLVD128,想用2片来实现,但是芯片输出的是MLVDS差分标准,能直接接到FPGA的LVDS接口上吗?有没有更好的方案或其他芯片来推荐呢,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有一路50M的时钟信号需要转成16路同步的LVDS差分时钟信号走背板给FPGA芯片,我看了一下SN65MLVD128,想用2片来实现,但是芯片输出的是MLVDS差分标准,能直接接到FPGA的LVDS接口上吗?有没有更好的方案或其他芯片来推荐呢,谢谢!
MLVDS和LVDS电气参数还是有区别的,比如驱动器差分输出电压幅值是不一样的。
TI有LVDS fanout器件,比如用于LVDS的data/clock 1:10的DS90LV110A 。如果需要16路的话,可以考虑使用两个DS90LV110A。
我查了一下,能用SN65LVDS387来实现我的方案吗?DS90LV110A比SN65LVDS387优势在哪里呢?
SN65LVDS387只是一款多路driver,不能实现fanout 1:16的功能呢。
我把SN65LVDS387的16路输入都接在一起就可以了吧?这样做有什么问题吗?
看一下 CDCLVD1216
支持LVCMos的输入,16路LVDS输出的clock buffer