我最近在调试SN65DSI83,发现一个问题是当我设置LVDS clock为70M的时候,芯片输出只有35M左右,设置为60M时,芯片输出只有30M左右,但是寄存器(0x0A)读取到的范围是对的,这是为什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我最近在调试SN65DSI83,发现一个问题是当我设置LVDS clock为70M的时候,芯片输出只有35M左右,设置为60M时,芯片输出只有30M左右,但是寄存器(0x0A)读取到的范围是对的,这是为什么呢?
使用外部时钟70Mhz给REFCLK还是使用DSI channel A clock提供LVDS clock?那么可看下寄存器0x0B的配置,是否将分频系数配置为2 了,导致2分频,输出为一半时钟。
Hi Kailyn:
我使用的是DSI channel A clock,频率为 351Mhz, 5分频后得到70.2Mhz的LVDS clock, 0x0B寄存器我设置的值是0x05,请问这样设置有问题吗?
有问题, 因为您是使用DSI Channel A clock,所以分频应该取决于是0x0B bit[7:3], 5分频的话为00100,0X0B bit[1:0]应该为00. bit2 默认为0的话,那么应当配置成0X20. 您试下。
sorry,我刚才的陈述有误,我的配置是:
{0x0A, 0x03},
{0x0B, 0x28},
稍后我将我的整个 CSR列举出来。