Other Parts Discussed in Thread: TXS0102
一个I2C接口,外接两个设备(1)TXS0102DCUR,(2)TSC2007IPWR。TXS0102DCUR主要用于HDMI总线上读取外部显示器的EDID,用于电平转换用,将处理器这边的3.3V电平转为HDMI设备的5V;TSC2007IPWR,用于四线式触摸屏。
现在有一种很严重的现象,将HDMI插到我们的板子上后,整个i2c总线死掉,HDMI无输出,触摸屏无反应。用示波器测得:SCL=0;SDA=1;另一种测的现象是:SCL有波形,但每一个时钟的电平呈下降现象:第一个3.3V,第二个3V,第三个2.4V……还有一种测得的现象是:SCL:2.4V;SDA:0.9V。都是非正常现象
不知这种现象是何种问题导致?