请问下可能的原因,怎么解决?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
它自身的ESD防护等级:2KV HBM,500V CDM。
COM接到VCC上了吧? 另外,外围有其他器件吗,静电测试只有ULN2003V12损坏?
COM接到VCC了。外围没有其他器件,静电测试只有ULN2003V12损坏了。
损坏之后,给ULN2003V12供电的12V电压被拉低到5V左右。
静电测试电压多少?您是怎么测试的呢?用的什么测试设备。
ULN2003V12只支持器件等级ESD,不等效系统ESD。
如果是进行IEC61000-4-2,直接ESD或者空气ESD,即使相同电压等级,也有可能出现损坏。因为IEC61000 ESD为系统ESD测试。
需要外围加ESD保护器件或者TVS进行额外保护。