请教下,DS90UB913A/Q, DS90UB914A/Q 支持的camera分辨率
从SPEC看其支持到10-bit 100MHz; 12-bit 75MHz
目前我有一个sony的camera sensor, 输出是1080p@30fps, 10bit 74.25MHz, 从SPEC来看是完全支持的。
请帮忙看看DS90UB913A/Q, DS90UB914A/Q是否可以支持1080p@30fps, 10bit 74.25MHz的应用
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教下,DS90UB913A/Q, DS90UB914A/Q 支持的camera分辨率
从SPEC看其支持到10-bit 100MHz; 12-bit 75MHz
目前我有一个sony的camera sensor, 输出是1080p@30fps, 10bit 74.25MHz, 从SPEC来看是完全支持的。
请帮忙看看DS90UB913A/Q, DS90UB914A/Q是否可以支持1080p@30fps, 10bit 74.25MHz的应用
您好!
913可以支持您的需求。
另外推荐933,和913是Pin-pin的,但是传输能力更强。
DS90UB913A/Q 10bit payload能够支持的pixel clock最大为100Mhz,所以1080p@30fps, 10bit 74.25MHz的应用没问题,能够支持。