tms320c6678的io电压1.8V,fpga的3.3V,连接两者时之间需要加什么电压转换芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tms320c6678的io电压1.8V,fpga的3.3V,连接两者时之间需要加什么电压转换芯片?
不知您需要几路的,信号速率最高多少。
您先参考这两款:
8路的话您可以参考SN74LVC8T245,四路的话SN74AVC4T245.
你好,
FPGA 一般不同的IO 的Bank可以采用不同的供电电压,是否可以考虑对于DSP连接的bank 采用1.8V 供电。