Other Parts Discussed in Thread: DS90LV110T
我正在设计一个主板对接8块子板的系统,主板上有一个总控,需要对8块子板分系统进行时序控制,控制信号是4对LVDS差分信号对,通过航天插座到转接板上进行1路分8路的转换。信号速率不高,也就10M左右,请问TI有这种LVDS信号1路转多路的芯片吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90LV110T
我正在设计一个主板对接8块子板的系统,主板上有一个总控,需要对8块子板分系统进行时序控制,控制信号是4对LVDS差分信号对,通过航天插座到转接板上进行1路分8路的转换。信号速率不高,也就10M左右,请问TI有这种LVDS信号1路转多路的芯片吗?谢谢!
你好,
请参考芯片DS90LV110T,为1:10的LVDS 数据/时钟分配器
感谢推荐!我看了下芯片手册,有个不明白的地方请教。我的设计中,主控板上的LVDS是由FPGA的HP管脚,就是电平等级是1.5V的LVDS,通过该芯片分路后,进入分系统的板上的FPGA,是应该用1.5V的HP管脚,还是应该用2.5V的HR管脚。简单地说,就是这个LVDS分路器会不会改变我分路前的信号电平等级呢?
你好,
首先要确定是采用直流耦合方式还是交流耦合方式,直流耦合就要多考虑共模电压是否匹配;其次是差模匹配,只要主板FPGA HP配置输出的LVDS 电平差模范围在分系统板LVDS 接收识别范围内就没有问题。
感谢您,Shawn Ding。我主控板用的FPGA是V7系列690T,由于它只有HP(电压等级1.2V到1.8V),分系统用的FPGA是K7系列410T,它有HP和HR(电压等级1.8V到3.3V)。如果我两边选择都是HP的管脚做LVDS信号的输入输出,他们的LVDS电平差模应该是匹配的,电压等级我也可以选择一样的。我想问的,也是我不确定的就是这个LVDS分路器会不会改标的电压等级?导致两边的HP管脚电压不匹配了。感谢回复。
单纯就DS90LV110 来说,它的输入输出共模电压是不变的。如果和后端receiver 连接的共模电平不匹配的话,那需要AC耦合方式。 重新通过电阻分压的方式建立能够满足reciever的共模电压。如果和后端receiver共模电压相同,可直接采用DC耦合方式连接。