This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
购买过LMK04808B时钟验证板,通过CodeLoader界面配置好,当全部Load bits后,在RUN,发现bits无法加载到LMK04808B板子上,同时使用示波器测试USB2ANY HPA665端口出来的data信号和clk信号,发现clk信号正常,而data信号是连续的脉冲波?
你好,
我将你的问题转到E2E上去了,请查看此链接内容
https://e2e.ti.com/support/clocks/f/48/t/638126
试了好几天了,无论使用哪些方法,都无法把bit加载到LMK04808B开发板,CPout1,Cpout2有时候是1.65V电平,有时候是0电平,其它的CLKOUT很多时候是没有输出的,只有CLKOUT6和CLKOUT8有122.88输出,通过插拔PC机上的USB口,发现LMK04808B板子上消耗的电流有变化,同时有时候几路CLKOUT有高电平或者意想不到的频率时钟输出???
不是只能使用OSCIN作为输入时钟源,CLKIN1也可以作为输入.一个是PLL2的参考输入,一个是PLL1的参考输入.
无法加载有可能是port配置不对导致不能正常加载.
另外,E2E上建议您使用TICSPro,用这个试试看能否正常加载.
http://www.ti.com/tool/TICSPRO-SW?keyMatch=TICSpro&tisearch=Search-EN-Everything
我的意思是在LMK04808B开发板上,只使用自带的OSCIN作为122.88输入时钟源,而CLKIN1不接任何输入,按操作步骤能否加载bits,另外我的Port是从76页到78页调接帽接的,这bits无论如何也加载不进去