Other Parts Discussed in Thread: TXS0104E, TXS0108E, TXB0108
硬件设计电路为1.8v-3.3v转换电路,外围连接总线已经断开,该芯片上电就会持续输出如图中的电平,请教为什么
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我看您这里OE直接拉高使能了,建议上电过程,OE是一个由低到高的变化过程,或者说等power stable之后,再将OE拉高。
如果输出还是这样,请反馈。
已经对该引脚做了控制实验,但是并没有效果,使能时仍然会出现这种现象
检查下焊接情况呢,因为外围电路都已断开, 单纯的验证芯片功能,看电路和应用都没问题。
另外,3.3V黄色波形是输入?现在3.3V到1.8V转换方向不正确是吗?
TXS0108和TXS0104的区别在于通道数不同,内部架构是相同的。
这样看来很有可能是TXS0108自身的问题,换了新的也是出现同样的问题,一上电就出现这种问题是吗?
在TXS0108E的产品主页上可进行样片申请:http://www.ti.com.cn/product/cn/TXS0108E/samplebuy
点击“样片申请” 登录my.TI账号,完善信息进行申请。
TXB0108是否可以用在UART电平转换上面,在现有电路基础是否可以直接做替换,需要怎加上啦电阻吗?