各位TI的大神,麻烦帮忙解决DS90C387调试问题:
使用335X平台输出RGB信号,通过DS90C387转换为双路LVDS接口信号,通过排线连接到显示面板驱动22英寸显示屏问题如下
1、单色显示正常
2、平均分7行显示7种颜色,显示正常
3、平均分7列显示7种颜色,不同颜色相交处抖动,花屏
4、显示图片,只有大概的轮廓,花屏
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LCD的分辨率是多少? 在靠近LCD端是否有端接100ohm匹配电阻?
另外,可以把DS90C387的电路附上,先看下电路图。
恩,两点需要确认:
1. LCD的frame rate是多少?1920*1080P@60Hz的分辨率的话,需要pixel clock频率为148.5Mhz。
那么DS90C387在single to dual mode中,能支持到170Mhz。所以要看下jumper中DUAL您是怎么配置的,需要将DUAL配置成1/2Vcc即可。
2. 就是data mapping是正确,请参考datasheet 中Page19 有关single to Dual mode的data mapping,因为附件电路您是将48bit RGB改为24bit,所以需要确认data 连接是否正确。。