Other Parts Discussed in Thread: TCA4311A
TCA4311A的EN为高,VCC电源也正常,但是ready输出一直为低?请问是什么情况!总线上其他节点正常!
1000片出了10片这种情况!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TCA4311A
TCA4311A的EN为高,VCC电源也正常,但是ready输出一直为低?请问是什么情况!总线上其他节点正常!
1000片出了10片这种情况!!!
这款芯片使用起来不复杂,您目前出现的这种现象建议做下交叉实验,比如将不正常的TCA4311A更换到能正常工作的板子上,或者将正常工作板子上的TCA4311A换到不正常工作的板子上,验证是芯片的问题还是板子的问题。
可以根据ready Vol (max)=0.4V,在Ipull up=3mA的测试条件下计算一下。goodluck xu 说:请问,如果ready的上拉电阻为1K ,芯片会不会烧毁!
(Vcc-0.003*Rpull)/Rpull< 0.4V
经过计算Rpull>8ohm即可。
所以上拉1K是没问题的,datasheet中推荐的是10K。
(Vcc-0.003*Rpull)/Rpull< 0.4V,这个方程好像不对吧,不应该再“/Rpull“
是的,不好意思。把分母去掉,这样计算下来Rpull约大于967ohm。goodluck xu 说:(Vcc-0.003*Rpull)/Rpull< 0.4V,这个方程好像不对吧,不应该再“/Rpull“