This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

生产1300个,有15个TCA4311A损坏问题求助

Other Parts Discussed in Thread: TCA4311A, TCA4311

---------------------------------------------------------------------------------------------------------------------------

-----------------------------------------------------------------------------------------------------------------------

如图,背板使用TCA9548,插入IO板使用TCA4311A,实现IO板的热插拔功能,

其中,IO板的+3V3电源是背板检测到IO板可靠插入信号BOX1SET-P为200ms低电平时,通过+3V3_Cut1置低电平,给IO板提供+3V3_I2C。

背板的+3v3电源只要开机就有,未做任何的通断控制,即开机后,SCL与SDA背板一直通过上拉电阻接+3V3。背板与IO板未使用长短针连接器。

现象:

目前生产了1300个,有15个TCA4311A损坏。有几个是插入IO板后就不能向IO板的存储器写入数据,换了TCA4311A后,IO板可写入数据。有几个是插拔3次左右就不能向IO板写入数据,同样换了TCA4311A就可以向IO板写入数据!

请问:

1、电路原理上会不会造成TCA4311A的烧毁!

2、背板和IO板的电源线与通信总线为使用长短针连接器,对电路有什么影响?

3、另观察采购到的芯片表面都有两行印字,54TI和6KS,但是有一个损坏的芯片表面只印有54,其他的字母在放大镜下看不到,这种现象正常么?另外这种现象怎么才能出现?出厂的时候marking code会出现未印的情况么?

  • 失效问题请直接联系你们的供货商。

  • 单看TCA4311的原理图,供电正常,输入输出钳位电流最大不超过50mA是不会造成烧坏的。

    这里有一个问题,虽然您这里提供的TCA4311的每个引脚定义都没问题,但引脚排列上跟DGK封装是对应不上的,Pin1是EN引脚没错,但是实际在芯片的第一引脚,也就是和Pin8对着的都在第一行。

    可以对照有问题的TCA4311排查下这个问题。 丝印方面我们无法提供信息, 因为我们辨别真伪的唯一途径就是看购货渠道是否是通过授权代理商。