This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connect between LVPECL & VML

Hi,

 

We use TLK 2541, and the signal input from optical module.

The output is LVPECL.

The input of TLK2541 is VML.

 The TLK2541's input common mode range is from 1000 mV to 2250 mV

The output swing generated by optical transceiver is 800mV

The common voltage generated by optical transceiver is about 2000mV.

Our schematic attached. But it seems that the swing is too small.

We try to connect them directly, it not works.

How to connect with them if we want to use DC couple?

 

Thanks.



 

x 出现错误。请重试或与管理员联系。
x 出现错误。请重试或与管理员联系。
x 出现错误。请重试或与管理员联系。