Other Parts Discussed in Thread: CDCE949, CLOCKPRO
在使用cdce949是遇到以下几个问题:
1)i2c写操作时,器件无响应(ack),不知道是什么原因?同样的程序读写其他芯片没有问题。地址是0x6c。
2)具体操作寄存器就按照手册中来么?值配置npqr这几个值就好么?还是需要配置别的地方呢?
3)是否有现成的参考demo可供参考?手册中提到的感觉太简单了。
4)还有就是关于输出频率和目标频率之间都有什么关系?有什么不同?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1)7bit从机地址需要左移一位,即为0XCA。
2)寄存器的配置可以使用ClockPro software来帮助配置。http://www.ti.com/product/CDCE949/toolssoftware
3)这款有demo板子,如果自己做的板子,可以使用Clock Rro software帮助进行寄存器配置。
4)您所说的目标频率是输入参考频率?
说的目标频率是fvco,输出频率是fout,这两个频率之间有何区别?我最终该用哪个频率作为我的使用频率?
fout是输出频率。
按照手册28页公司1就按fout。
fvco是芯片内部的vco要满足的频率
我按照您提供的软件进行寄存器配置,但是y4输出还是27m,还有什么地方需要注意的么?我的操作仅仅是写了几个寄存器。