This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电平不一致还是不建议的,建议使用统一的VDDIO,要么是1.8V ,要么是3.3V。
如果前端image sensor是1.8V的话,建议先转成3.3V再和934连接。
GPIO 以及I2C 信号都是通过VDDIO 供电的,即使DES,SER的VDDIO不一致,但差分信号的传输不会造成影响,我担心的是I2C的双向通讯会不会有问题。
最好实际验证一下。
好的,非常感谢回复!
但是既然差分信号的传输不会受影响,从934到933的IIC通信也是通过同一通道传输的,应该也不会受影响吧?
目前板子正在生产过程中,有进展会及时在论坛更新的