This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ32002 晶振不起振问题32.768khz

Other Parts Discussed in Thread: BQ32002, BQ32000

請問一下各位大大, BQ32002的晶振没起来 ,是不是因为我没配置好所以他才没起振呢?那么BQ32002的驱动在哪里可以找到呢?

  • http://www.ti.com.cn/product/cn/BQ32000/toolssoftware

    可以在此链接下载驱动程序

  • 非常非常感谢您呢!已经下载完毕,并且集成进代码,以下是我的初始化代码:

    int bq32k_probe( void )
    {
    uint8_t reg;
    int error;
    struct rtc_time tm;
    i2cUtilsInitParams_t i2cUtilsParams = I2CUTILSINITPARAMS_DEFAULT;
    I2CUtilsInit(RTC_I2C_INST, &i2cUtilsParams);

    CONSOLEUtilsPrintf("bq32k_probe...\n");

    /* Check Oscillator Stop flag */
    error = bq32k_read(BQ32K_SECONDS, 1, &reg);

    CONSOLEUtilsPrintf("BQ32K_SECONDS = 0x%X. error = %d\n" , reg, error);

    if (!error && (reg & BQ32K_STOP)) {
    CONSOLEUtilsPrintf("Oscillator was halted. Restarting...\n");
    reg &= ~BQ32K_STOP;
    error = bq32k_write(BQ32K_SECONDS, 1, &reg);
    }
    if (error)
    return error;

    /* Check Oscillator Failure flag */
    error = bq32k_read(BQ32K_MINUTES, 1, &reg);

    CONSOLEUtilsPrintf("BQ32K_MINUTES = 0x%X. error = %d\n" , reg, error);

    if (!error && (reg & BQ32K_OF)) {
    CONSOLEUtilsPrintf("Oscillator Failure. Check RTC battery.\n");
    reg &= ~BQ32K_OF;
    error = bq32k_write(BQ32K_MINUTES, 1, &reg);
    }
    if (error)
    return error;

    /* Important
    timearrw[0]=0x5e;
    timearrw[1]=0xc7;
    timearrw[2]=0x01;
    bq32k_write(0x20, 3, timearrw);*/

    return 0;
    }

    现在的问题是,晶振可以了,但是:

    1. 为什么下电之后时间还是会回到之前的值呢,是0H:30M:24S。而且您看我配置函数里面,我都没有配置过。这是什么原因?

    2. 如果要时间继续走,那么还需配置哪些寄存器,具体要写什么值进去呢?

    请您帮忙回答一下好吗?谢谢您

x 出现错误。请重试或与管理员联系。