This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不能接10G 光模块呢,因为TLK2501 最大能够支持的速率为2.5Gbps。
您可以考虑TLK10031,最大速率可达10.3125Gbps,可以和10GBASE-SR或10GBASE-LR连接。
您好,主要是看中了TLK2501 16:1的串行/解串特性,另一端是带有SFP+的FPGA板卡,希望实现TLK2501与该板卡的通信。
即实现 FPGA (16bits并行数据)<—> TLK2501 <—> SFP+光模块 <—————> SFP+光模块<—>FPGA(集成收发器) 这样的结构。
不知采用2.5G的SPF+光模块,是否可以实现?
非常感谢!