This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我司项目使用了TUSB542芯片做Type-C正反插USB3.0信号开关,在Redriver调节这里,设定了最大De-Emphasis 6dB与最大Equalization 9dB;
现在发现一个现象,对于某些OTG设备,会出现正插识别反差不识别现象。
分析后,我发现把TUSB542的Redriver的CONN端TX的De-Emphasis设置为-3.5dB,问题解决。
我现在的疑问:是不是在对于所有串行高速信号,在TX端做了De-Emphasis的话,信号本身的高频分量不变,只是削减了低频(直流)分量,那么在Receiver端接受的信号高电平1的幅值会变低?从而出现了接收机接受灵敏度较差时,会出现通讯失败的现象?
也就是说是不是对于串行器件,De-Emphasis的增益设置并非越大越好?
希望得到权威解答,同时欢迎大家探讨,谢谢!