你好:
本人在查看TUSB8401 的 datasheet 时发现其中提到64脚需连接一颗 9.53k 1% 的电阻,不知其作用。
同时发现在有USB3.0的场景中均出现该类型电阻,希望老师们能解答下我的疑惑,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
本人在查看TUSB8401 的 datasheet 时发现其中提到64脚需连接一颗 9.53k 1% 的电阻,不知其作用。
同时发现在有USB3.0的场景中均出现该类型电阻,希望老师们能解答下我的疑惑,谢谢!
没有找到TUSB8401的芯片
认为是笔误,应该是TUSB8041
Precision resistor reference. A 9.53-kΩ ±1% resistor should be connected between USB_R1 and GND.
不仅仅在USB3.0,在USB 2.0 中也有这个电阻。比如TUSB4041这颗2.0的HUB中也有。
这个引脚,以及这个电阻的作用控制着USB2.0 或USB3.0 PHY的驱动能力,应该是经验值。 但是找不到对应的其他阻值与驱动能力的曲线。 在design的时候,建议采用这个值,不要使用10Kohm或其他阻值。