This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用方案是TFP403--->SN75LVDS83C
Q1:LVDS接1024x600分辨率:9.7‘屏,而PC这端分辨率一般为1024x768,这个差异如何解决,怎样沟通过tfp403解决?
Q2:LVDS这边也要接其他分辨率,tfp403可自动调节吗
Hi junliang,
Van Yang 的说法正确,这种分辨率的微调,在LCD display controller可寄存器设置调整,自动调节比较困难。需要先检测输入格式。
非常感谢大家的回复
目前项目简化要求支持1024*600的分辨率,但是有些显卡DVI输出不支持这种分辨率,就会导致显示异常,DVI如输出800*600,LCD的宽边会有224区域无显示,;DVI如输出1024*768,LCD不没法显示完整。
Dear Van
你说的控制行场同步,具体是怎么实现的
Dear Jeff
你说的LCD display controller可寄存器设置调整,这是要在LCD端调整吗
根据你的需求,需要系统具有scaler(缩放)功能,一般图形芯片具有这个功能。TFP403是纯物理转换,没有这个功能。
SN75LVDS83C直接驱动panel?如果这样的话,需要TFP403之前具有scaler功能的芯片。