This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DP83848的问题

Other Parts Discussed in Thread: DP83848C, DP83848H

1.83848正常供电3.3V及复位正常 ,这时接上RJ45网线是不是就可以正常运行起来(在不与PPC440GP通讯),主要是验证自我检测是OK

2.83848工作在RMII模式,需要外挂个50MHZ的有源晶振,给到芯片的P34,我看到你们设计加了个芯片CY2305,一路给到83848,另一路给到PPC440GP,可不可以不用这CY2305芯片,用83848内部(P25)输出50MHZ给到PPC440GP

3.83848这个芯片的软件 是不是原厂出厂都已烧录好的,已经固化的

4.设计资料中83848有两种工作模式,一个是MII模式下RJ45接口处有加网络变压器,而RMII模式下没有加网络变压器,不知道有什么区别

  • 1. 您指的BIST测试是吗?两种方式,一种是芯片内部自环,一种是通过外部接一个测试治具来做loopback。内部loopback的话不用接RJ45网线,直接提供时钟即可。

    2.您使用的DP83848哪款,比如DP83848C,DP83848H,因为在P34,没有看到您指的PPC440GP?或者是哪篇应用手册上?

    3. 芯片软件没有烧录好。需要自己烧录。

    4. 具体哪篇资料呢? 

  • 如果是新设计,建议使用DP83822。

    针对DP83848的问题。

    1. 接上网线,不做软件驱动,可以确定的是链接是否成功建立。通过LED_LINK引脚的状态可以观察,或者通过寄存器0x01h BIT2 link status寄存器读到。

    2. 可以,P25输出50MHz使用的是RMII mater 模式,但是必须使用50MHz有源晶振。DP83822可以使用25MHz无源晶振。

    3. 83848是物理层,可以通过strap电阻进行寄存器上电配置。但是软件和MAC是在CPU或者DSP里面做。

    4. RJ45接口是MDI 差分输出的接口,和MII模式和RMII模式没有关系。如果需要通过以太网标准测试,变压器是必须的。

  • 对于83822和83848不是很了解,不知道明显的区别是什么呢?新设计中怎么就考虑用83822了呢?