TI工程师,你们好!现有一个使用问题,麻烦帮忙解答一下。我购买了一个LMK04828BEVM开发板,通过查看板卡实物和原理图,发现板卡上没有参考时钟,仅有一个122.88MHz的用于第一级锁相环电路的压控振荡器,但是当用codeloader软件下载程序后,最终的时钟输出端口依然会合成特定频率的信号,这是怎么回事?没有板上参考时钟也可以吗?而从外部输入参考时钟信号,无论输入什么频率,对时钟合成的频率都没有影响,请问外部时钟输入如何通过软件来切换?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师,你们好!现有一个使用问题,麻烦帮忙解答一下。我购买了一个LMK04828BEVM开发板,通过查看板卡实物和原理图,发现板卡上没有参考时钟,仅有一个122.88MHz的用于第一级锁相环电路的压控振荡器,但是当用codeloader软件下载程序后,最终的时钟输出端口依然会合成特定频率的信号,这是怎么回事?没有板上参考时钟也可以吗?而从外部输入参考时钟信号,无论输入什么频率,对时钟合成的频率都没有影响,请问外部时钟输入如何通过软件来切换?
应该是自己提供参考时钟CLKIN1, user's guide中是这样描述的:
2. Connect a reference clock to the CLKin1 port from a signal generator or other source. Use 122.88 MHz for default. Exact frequency and input port (CLKin0/CLKin1) depends on programming
并且电路中,CLKIN连接的是一个测试点,也就是说方便和外部参考时钟源连接的。
您测量的是哪个输出端口的频率?频率是24.576MHz?
谢谢您的回复,我还想进一步问一下,我们想让DCLKout0端口输出600MHz的时钟信号,外部参考时钟输入端口有三个,在都不加信号的情况下,依然能输出最终的600MHz信号,而开发板内部确实没有晶振,按照锁相环电路,122.88MHz那个器件属于压控振荡器而不是参考时钟,按理说是行不通的,还请您进一步解答一下。
另外,为什么配置文件无法固化到开发板上,只能在线下载程序?我们将来依照开发板来设计自己的产品,这个芯片怎么固化程序呢,现在在开发项目,准备选用这个时钟芯片,请帮忙指点一下,非常感谢!
不能固定到开发板上。一般是用FPGA或者MCU进行读写寄存器操作。