This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DS90UB914A/DS90UB913A配置问题

你好!我在913A端接了一个sensor ISP,输出8bit YUV422数据,ISP 芯片I2C地址是0X90,在914A端用主机接收同样格式(YUV422 8bit)的数据,请问如何通过I2C配置914A寄存器呢?依次需要配置哪些寄存器,寄存器值配置成多少?谢谢!

  • 配置914 就是主机和local I2C之间的通信,没有涉及到remote通信,因此相对比较简单。

    需要配置的寄存器为I2C Device ID,比如0X60.是由IDx引脚决定的。

  • 谢谢!我的意思是目前我主机可以直接接sensor ISP的DVP接口获取数据,sensor ISP上电默认有8bit YUV422数据输出,为了延长摄像头与主机之间的距离增加了913A和914A,主机从914A接收数据,硬件连好了就直接可以接收数据了吗,是否还需要通过I2C配置914A的寄存器呢?