This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD2E001-Q1

Other Parts Discussed in Thread: TPD2E001-Q1

你好,有个问题请教下,我们现在有个项目有用到贵司的TPD2E001-Q1做USB的D+,D-信号线保护,我们要求D+,D-和,USB5V都要和12V短接1分钟,考虑到这个种情况,我没有接VCC引脚接到电源上,直接是一个0.1UF电容到地,如下图。我在DATASHEET上看到有这段话,但不知怎么理解,是不是这个引脚不一定要接到电源上,可以直接通过一个电容到地。

  • 这段的意思是:
    1)如果VCC接电压的话,那么Vio的电压幅值最大不 能超过VCC+Vf, Vf最大电压为0.95V,Vcc最大为5.5V,也就是说Vio最大电压不能超过5.5+0.95V=6.45V。
    2)如果不接在电源上的话,Vio的电压幅值上限是10V。 不接的话,可以直接悬空。
    但二者的情况都建议加上0.1uF的去耦电容。
x 出现错误。请重试或与管理员联系。