This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04821 reference clock input problem

Other Parts Discussed in Thread: LMK04821

Is it possible to use one of clkin0 / 1/2 as a reference clock input for single-phase-locked loop mode?

THX

  • 可以,看下datasheet Figure10 的内部架构,可以看到内部集成MUX, 即使CLKIN0,1,2都有输入,也需要通过PIN CLKin_SEL1和CLKin_SEL1引脚来配置这三个通道哪个是active的。

  • 在使用单个pll时,如果我想采用内部的VCO0/1,那么我看datasheet Figure10的内部架构 我只能使用pll2,而 clkin0/1/2中只有clkin1复用管脚可以通过FB_MUX进入pll2_MUX,进而可以利用pll2使用内部的VCO产生想用的频率输出,,请教一下我这样理解是否正确?? 也就是说我想利用LMK04821设计成单pll的,只可以使用PLL2,而PLL2的参考频率可以为OSCin和clkin1. 对内部架构的理解是否正确 望指教下 。


    谢谢