This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好:
我现在使用CDCE62005使用参考时钟是25MHz晶振,想各路时钟分别为:125MHz;100MHz;250MHz;50MHz;50MHz;寄存器的值该怎么配?我根据软件配置总是125MHz为120MHz,其他路也是有成倍数减少比如,250MHz为240MHz。请问各位这是怎么回事?
Xiang
看一下手册的第23页。有一个例子是25M输入,125M输出的。你把输出divider减小一倍就输出250M了