This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE925 LVCMOS clock Input 能否使用有源晶振 40MH在配置输出至少两路40.96MHz信号?



之前电路使用26MHZ有源晶振 配置输出可以锁定输出两路40.96MHz信号和一路32.768MHz

最近更改为40MHz有源晶振,但是配置锁定始终失败,参数从软件得到输入的

  1. 向咨询这个款芯片能否使用有源晶振做时钟输入 尤其40MHz ?配置选项应当选择LVCMOS clock Input 模式?
  2. 电路使用是否应当在晶振一侧并联51.1欧姆到底完成阻抗匹配?还是需要增加两个100欧姆上下拉1.8V?
  3. 这样配置数据有无问题?这样工作是否可以正常?