This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RT
我司有种特殊需求,想使用前端FPGA将两个视频数据流(带两个VC通道),经过953后,经过FPD-LINK III传输,给后端的964,请问后端能不能根据VC通道号,分出两个视频流!谢谢
好的。
比如说我们前端使用FPGA的MIPI CSI-2 TX的一个X4Lane,连接到953上(模拟成一个FPD-LINK的相机),这个数据中包含两个MIPI CSI-2格式的视频流,分别使用VC=0 VC=1区分;对于954可以接2个模拟FPD-LINK相机,是否可以在后端成功解析出2个分别带有相同VC=0 VC=1的视频流;同样的问题,2个模拟FPD-LINK相机是否接进964后,能够把视频流区分开?