This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00301SQX到TMS320TCI6608ACYP的时钟匹配设计和验证求助咨询(紧急求助,感谢优先支持!)

1、设计电路如图,应该是属于LVPECL(确认驱动器输出为LVPECL) to LVDS的匹配吧。如果确认匹配没错,那么驱动器输出端,DSP接收端有什么具体的信号质量的要求呢?特别是DSP的接收端如何判断满足输入规格要求呢?

2、DSP端的信号要求是:

All differential clock inputs comply with the LVDS Electrical Specification, IEEE 1596.3-1996 and all SERDES I/Os comply with the XAUI Electrical Specification, IEEE

802.3ae-2002.

——摆幅要求多少(是否可以超过350mV,最大最小多少呢?),共模电压要求多少(比如标准值,最大,最小等等),对差分信号、单端信号的电平,判决有什么样的具体要求。
——目前聚焦这几个信号,CORECLKP /N,DDRCLKP /N,PCIECLKP /N

3、我在DSP模块也有求助,他们建议到接口/时钟模块咨询,感谢支持。

4、驱动器的单体差异,顺便帮我看看附图的2个波形是否都满足LVDS(DSP)的要求?(见附图的2个波形,摆幅有差异)

5、这几个文档我都没有找到具体的电平、判决、摆幅方面的详细要求,因此请帮忙确认下。

sprabi2c[keystone hardware design guide]

sprabi4[Clocking design guide for keystone device]

tms320tci6608