应用是做一个支持USB3.0的安防摄像机。考虑到USB传输质量的问题,且需要向下兼容USB2.0,想使用TUSB522P与TUSB211作为USB redriver。
1、不知这种组合方式是否有问题,或者有没有更好的推荐?
2、在查看TUSB522P的芯片资料的时候,发现芯片的增益均标示在2.5GHz的条件下,而USB3.0理论上来说带宽为5G,是否是说USB3.0在super-speed模式的TX和RX分别只有2.5G时钟频率?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应用是做一个支持USB3.0的安防摄像机。考虑到USB传输质量的问题,且需要向下兼容USB2.0,想使用TUSB522P与TUSB211作为USB redriver。
1、不知这种组合方式是否有问题,或者有没有更好的推荐?
2、在查看TUSB522P的芯片资料的时候,发现芯片的增益均标示在2.5GHz的条件下,而USB3.0理论上来说带宽为5G,是否是说USB3.0在super-speed模式的TX和RX分别只有2.5G时钟频率?
1. TUSB522P是USB3.1 redriver,专门设计用在5Gbps data rate的redriver,我还没见过用两个redriver的结合应用哈。 您需要很长的传输距离吗?如果考虑向下兼容的话, 可以考虑USB3.0 HUB,可以向下兼容,并且HUB能起到redriver的作用。
2. 2.5GHz的频率,即为5Gbps的data rate。
你好,谢谢~您的意思是USB3.1的redriver一般是不会向下兼容USB3.0和2.0么?USB3.0 HUB有redriver功能,那也行,有推荐哪颗不?我看了一颗TUSB8020B貌似可以,我主要是想用个两通道的usb3.0的redriver来改善USB3.0传输IPC视频时的图像质量,同时想能向下兼容USB2.0,之前看了这两颗SN65LVPE512 and SN65LVPE502x,TI官网都显示不推荐使用了,推荐用TUSB522P,也没找到其他支持usb3.0两通道的芯片,您有什么推荐或建议么?多谢多谢~