This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD芯片的钳位电压VC

Other Parts Discussed in Thread: ESD122

ESD芯片的钳位电压VC要小于保护器件的最大允许电压,这个最大的允许电压有别于芯片的最大电压,芯片的最大电压是一个直流量,芯片管脚最大的允许电压(100ns脉冲的)这个值去哪里查找呢?貌似芯片的数据手册上没有写

  • TVS的最大钳位电压VC应低于被保护电路所允许的最大承受电压,而被保护电路所允许的最大承受电压由您的外部电路所决定,在TVS芯片 datasheet没有这个参数。
  • 有些比较旧的ESD芯片上没有给出TLP的有关信息,您说的这个信息在新产品ESD122中有给出TLP response 曲线,可以详细了解一下:
    www.ti.com/.../esd122.pdf
  • 是的,现在困扰我的两个问题:
    1.TVS芯片选多大功率的,因为TVS芯片的功率决定了IPP,我不清楚外部的静电或者浪涌的电流是多大,因此不知道该选多大功率的TVS芯片;
    2.选多大钳位电压的TVS芯片,当然TVS芯片的钳位电压越低越好,问题是我如何确认被保护电路的最大允许电压值,比如我要用TVS保护USB电路,我如何确认USB电路的最大允许电压值?一般的芯片手册会给出USB最大的电压值,但是这个值一般是个直流电压,而TVS保护的是100ns左右时间的尖峰电压,USB芯片的数据手册中很少会提及这个参数