This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954:请问954、953该如何去配置?

我现在的摄像头规格如下:

分辨率:1920 X 1080;

帧率:30;

lane数:2lane; 

数据格式:CSI    RAW 12bit;

 

954 配置:

1:VDDSEL = 0 1.1V采用内部LDO

2:IDX 10K下拉 上拉NC I2C address: 0011 000x

3:mode 78.7K 上拉 97.6K 下拉

953配置:

1:IDX 40.2K 下拉

2:mode 下拉4780 NON-Synchronous mode

 

目前摄像头MIPI信号已出,但954那边没MIPI信号输出。感谢支持。

x 出现错误。请重试或与管理员联系。