This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925 和DS90UB926IIC通信异常

Dear TI FAE,

    产品链路:MCU----》925----STP线------》926

   遇到的问题:MCU通过IIC可以配置925,并且ds90UB925的寄存器0x06里面可以读到926的Device ID 0x58,cable link已经建立。但是接下来要如果操作哪些寄存器来配置926,目前无法通过925来配置926.

 请不要建议参考snla222,因为913和914的配置比较简单是因为913/914的寄存器0x06和0x07有 Des Alias/Ser Alias这个选项,但是925和926没有, 已经尝试过all pass-through 模式,但是依旧是无法配置926(将0x58作为926的设备地址进行IIC读写异常。)

  非常感谢!