This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CF386MTD此芯片是否兼容6 bit LVDS信号(D0+ D0- ,D1+ D1- ,D2+ D2-,DCLK+ DCLK-)输入?

Other Parts Discussed in Thread: DS90CF366

请教问题:请问DS90CF386MTD此芯片是否兼容6 bit   LVDS信号(D0+ D0-  ,D1+ D1- ,D2+ D2-,DCLK+ DCLK-)输入?    如果兼容,要怎 么应用?软件,硬件注意哪些方面?
   (目前我们用8bit   LVDS信号(D0+ D0-  ,D1+ D1- ,D2+ D2-,D3+ D3-,DCLK+ DCLK-),输出TTL正常。用6 bit   LVDS信号(D0+ D0-  ,D1+ D1- ,D2+ D2-,DCLK+ DCLK-)时屏幕显示较暗)
  • 可以的,也就是说需要3 对LVDS 信号和21bit LVCMOS 并行数据输出是吗? 就和DS90CF366功能一样。
    data mapping上,可以将 RxIN3± 直接端接100ohm匹配电阻,然后直接悬空。无需上下拉。
    另外,RGB这边,需要将高两位悬空,比如R6,R7,G6,G7,B6,B7 悬空。 所以检查下电路引脚连接情况。