电平转换芯片手册上写的极限参数都是每路输出正负50ma,但是VCCA、VCCB和GND的持续电流是正负100ma(2、4和8路都是100ma)。那如果使用的是8路的芯片,是否整体电流就需要控制在100ma以内。因为现在的产品使用的是8路的芯片,现在发现整体电流会超过100ma(暂时使用还没有问题)。但是分成4路的话就不会超过100ma,所以是否需要更换?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电平转换芯片手册上写的极限参数都是每路输出正负50ma,但是VCCA、VCCB和GND的持续电流是正负100ma(2、4和8路都是100ma)。那如果使用的是8路的芯片,是否整体电流就需要控制在100ma以内。因为现在的产品使用的是8路的芯片,现在发现整体电流会超过100ma(暂时使用还没有问题)。但是分成4路的话就不会超过100ma,所以是否需要更换?
之前用的SN74LVC4245A,手册上的推荐IOH IOL是小于24ma。现在用的最大情况也就在30ma左右,但是即使只有20ma的话,如果超过5路时ICCA就超过100ma了,因为是2 4 8路的芯片ICC极限都是100ma,我的意思是如果用2路或者4路的是不是就没有隐患了。我看到还有SN74LVC8T245的 IOL和IOH达到了32ma,可多路一起工作也很容易超了ICC的极限?所以说要8路都工作的话IOHIOL就没有参考意义了吗?因为现在空间有限,现在如果换成2颗或者3颗芯片空间上就有点限制。