This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947使用疑问

1、使用DS90UB947输入使用一路LVDS,使用输入接口D0+/-  ——  D3+/-和一组CLK+/-,输出使用单路链接,需要实现SXGA(1920*720)/30fps/24bit这个需要将像素时钟设置为多少?

2、DS90UB947的参考设计,DS90UB947的49引脚 INTB是通过了电平转换控制的,我们是否可以直接使用3.3V直接上拉?

3、DS90UB947的参考设计,DS90UB947的31引脚 PDB是通过了电平转换控制的,由于我们不使用这个功能,请问是否可以悬空处理?

  • 1. 首先947 是肯定支持这个分辨率的,因为单link支持到96MHz,双link能支持到170Mhz。而这个像素时钟不是947 来设置的,是前端视频源来决定分辨率的。
    2. INTB为开漏输出,建议上拉4.7kohm到VDDIO。 而VDDIO最大不能超过1.89V,典型值为1.8V,所以上拉倒1.8V。
    PDB同样也是,不能直接悬空,建议上拉10KOhm电阻到VDDIO。参考datasheet 10.1 部分有关上电时序的介绍。