This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CF364实现LVDS转DVI的问题请教,急等回复!

Other Parts Discussed in Thread: DS90C363, DS90CF364

工控主板前端是采用DS90C363芯片把RGB565格式转为单6的LVDS信号输出, 

目前想实现的功能是把LVDS信号,经过DS90CF364芯片转换为TTL电平的RGB信号+SII164CTG,实现LVDS转DVI的功能,

问题1:请问这样连接是否有问题?

问题2:目前板卡调试的过程中,图像基本没有显示,只有偶尔的一次才能看到图像,是不是RGB565格式无法直接与RGB888的芯片对接?

问题3:DS90CF364输入端匹配有100欧姆的电阻,输出端TTL信号线全部等长,并且信号线串联有33欧姆的电阻,这样配置是否合理?

问题4:DS90CF364芯片是否是自适应的始终上升沿还是下降沿采样功能,芯片介绍里没有提及(示波器测量DS90C363的TTL输入时钟和DS90CF364输出的TTL时钟图形,正好相差半个周期,请问是什么为题造成的?)

  • 1. 使用SD90CF364和DS90C363搭配使用没问题,DS90CF364 可以实现1个channle的LVDS 转21bit TTL 输出,其中18bit RGB+3 control signal。按照您的描述,需要LVDS to RGB888的转换吗?或者说SII164CTG是RGB888接口?
  • 2. 输入差分端端接100ohm匹配电阻没问题,输出串联33ohm可无。
    4. 这款不带自适应或者均衡功能。
x 出现错误。请重试或与管理员联系。