工控主板前端是采用DS90C363芯片把RGB565格式转为单6的LVDS信号输出,
目前想实现的功能是把LVDS信号,经过DS90CF364芯片转换为TTL电平的RGB信号+SII164CTG,实现LVDS转DVI的功能,
问题1:请问这样连接是否有问题?
问题2:目前板卡调试的过程中,图像基本没有显示,只有偶尔的一次才能看到图像,是不是RGB565格式无法直接与RGB888的芯片对接?
问题3:DS90CF364输入端匹配有100欧姆的电阻,输出端TTL信号线全部等长,并且信号线串联有33欧姆的电阻,这样配置是否合理?
问题4:DS90CF364芯片是否是自适应的始终上升沿还是下降沿采样功能,芯片介绍里没有提及(示波器测量DS90C363的TTL输入时钟和DS90CF364输出的TTL时钟图形,正好相差半个周期,请问是什么为题造成的?)