This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB211/212/213/214/215

Other Parts Discussed in Thread: TUSB212, TUSB211, TUSB213, TUSB214, TUSB215

Dear All,
请问 TUSB211/212/213/214/215的区别在哪里?哪一个更适合高速的传输速度?

  • 区别如下:
    TUSB212 adds DC boost and can support longer channel than TUSB211.

    TUSB213 is a 5V supply part and supports 5V voltage protection, it also has DC boost and can support long channel .

    TUSB214 is a 3.3V supply part and supports CDP. it also has DC boost and can support long channel.

    TUSB215 is also a 5V supply part and supports 5V voltage protection and CDP. it also has DC boost and can support long channel.
  • 在传输速度上是没有区别的是吗?
  • 是的,传输速度上没有区别,都是支持USB2.0 480Mbps的标准。
x 出现错误。请重试或与管理员联系。