This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

913使用外部时钟模式,12-bit高速模式,外部晶振为50M(GPO3),GPO2为什么不能输出25M时钟?求大神帮忙,谢谢



913使用外部时钟模式,12-bit高速模式,外部晶振为50M(GPO3),GPO2为什么不能输出25M时钟?

914:VDDIO为3.3V

SEL为低电平

PDB为高电平

OEN为高电平

OSS_SEL为高电平

LOCK为低电平

PASS为低电平

BISTEN为低电平

MODE:3K下拉,12位高速模式

913: VDDIO为1.8V

MODE:4.7K下拉,外部时钟模式

PDB为高电平

  • GPO2 输出是多大频率?那么相应的image sensor输出的pixel clock也不是75Mhz了吧?
    另外,914的VDDIO我看是3.3V, MODE引脚的10K电阻需要上拉到1.8V,而不是VDDIO,所以注意不要上拉到3.3V就行。
  • 你好,所有电压已经根据他们的数据手册检查过了,没有问题,GPO3测量是50MHz ,GPO2测量没有输出任何频率(理应输出25MHz)。

    我的问题是:为什么GPO2没有25MHz?

  • 恩,也就是说GPO2没有任何输出,我的本意是以为输出其他频率的输出,所以想和您确认下GPO2输出的是多大频率输出,从而判断GPO2作为sensor的参考输出的pixel clock又是多大。

    既然GPO2没有任何输出,那么需要从PDB入手,看是否913 还是处于power down状态,因此要确认下PDB是否为高电平,另外建议PDB 遵守上电时序,当VDD和VDDIO电压都起来到稳定之后PDB再拉高。