This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848 RMII模式下RMII_REF时钟问题

您好!

        我们选用DP83848的RMII工作模式,控制PHY 芯片的CPU在一个小扣板上,底板上有两个DP83848。50M的时钟又在扣板上的有源晶振提供,经过一个时钟buffer后,一路输出到到扣板上的CPU,另一路输出经过接插件到底板上,再经过有使能控制功能的时钟buffer输出两路时钟信号,到两个DP83848。底板上的时钟buffer最大的输入输出延迟有5ns,再加上时钟到CPU那一端的线要比到底下PHY芯片的线要端,这样会不会导致掉包?RMII模式下到CPU和到PHY芯片的时钟延迟最大很接受多少,才是安全的?多谢!

  • 您的意思是,时钟信号到CPU要比到DP83848的时间快很多,通过描述,50MHz有源晶振经过buffer输出直接给CPU,而给两个DP83848的时钟经过底板,又经过另一个buffer输出才到DP83848? 这样的话,整个链路的jitter以及信号衰减要考虑进去。
    那我想,为什么不直接使用一个三路输出的buffer,一路给CPU,两路直接输出给DP83848?
  • 因为那个扣板早就做好了,当时没有考虑到之后会用RMII的那种模式。底下有一个buffer是想使用它的使能引脚,在需要的时候去停止PHY的时钟。
  • TI这边有没有那种延迟很小的时钟buffer推荐的。是不是时间延迟做到一定范围内,就没问题了,我看了DP83848的那个datasheet上RX上的数据比那个参考时钟最大要延迟14ns,是不是意味着留给CPU的建立时间最多就6ns?超过这个就会有可能掉包吗?
  • 我看了datasheet上写了RX上的数据最大比参考时钟要慢14ns,这个是不是意味这留给CPU的建立时间只有最多6ns,超过就会掉包吗?