This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2.0 TYPE-C 接口

大家好,我们想使用USB2.0连接到type-c物理接口。有以下几个问题:

1.如果只是作为Device角色,是否可以像普通的microB接口一样,D+,D-,VBUS,GND,连接到相应的pin上。而CC引脚直接用电阻下拉到地。其他是否需要做任何特殊处理。

2.如果按照第一种假设,在对此device进行充电时,是否有其他通信问题?(比如线的另外一端分别是type-a,type-c,和microAB)

3.如果是做OTG连接到type-c上,是不是一定要用相应的逻辑芯片,来使CC通信决定角色?

4.如果是上述假设,cable的另外一端是microB的device,而之前的device想通过OTG的方式做HOST。请问这样的情况下怎么实现?因为type-c上没有ID线。而microB那一端又没有CC线。