This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ds90ub954 拉低IIC电平信号,发送端DS90UB913. IIC配置不了

问题是偶发性,有时出现一个情况 host端无法个954 i2c无法通信,host无法发起start信号? 导致DS90UB954没有法配置通讯. 

1. 问题一,DS90UB954 出现异常是否会拉低IIC信号?

2.出现问题时软件复位主控,iic复位不了,是否有办法复位DS90UB954芯片?

  • 1. 拉低I2C信号具体指的是? SDA和SCLK均为低电平?
    2. 如果是想复位寄存器为默认值的话,可以通过硬件复位,即PDB引脚由高到低的变化过程,也可以通过软件复位,即寄存器Reset (Address 0x01)