This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用ARM的CPU输出Maximum VCLK in RGB Interface :80MHZ,24bitRGBLVCMOS数据(1.8V),想要驱动显示双8屏(DCLK最小 48MHZ)。所以想采用DS90C187,来转换数据,不知道这样能不能实现,会不会80MHZ的时钟驱动不了双8屏(DCLK最小 48MHZ)。
试试看TI的FDPLINK 产品,比如DS90C383B
1、先前我打算采用SN75LVDS83,该芯片是支持1.8V的输入信号,但是该芯片只有单8位LVDS信号。我的是双8屏,所以想采用两个SN75LVDS83,可是不知道如何接线,也不知道能不能实现。
2、后来我打算采用DS90C387,该芯片有Single Pixel In Dual Pixel Out功能,但是发现该芯片是3.3V 数据输入。我需加两个电平转换芯片。
3、现在打算采用DS90C187,用Single Pixel In Dual Pixel Out功能,但是CPU输出Maximum VCLK in RGB Interface :80MHZ,不知能否正常点亮双8屏
DS90C187是最好的选择,功耗极低,从你给出的条件应该可以实现。