Other Parts Discussed in Thread: ISO3088, TXS0108E, SN74LVC4245A, LSF0108
各位专家有几个问题想确认一下:
1、TXS108E可以用做SPI、I2C总线的电平转换吗,PCB走线长度有限制吗?我是想板卡1通过TXS108E转将3.3换成5.0V电平,通过背板链接到板卡2,再用TXS108E转换成3.3V电平供3.3V系统用,或者是板卡2直接用5.0V的SPI、I2C接收芯片。主要是想提高电平,提高抗扰能力。
2、TXS108e可以直接链接用在一些接口芯片比如ADM2483、ISO3088、以及IS01050之间的RX/TX之间的信号电平转换吗,主要还是想提高信号电平,提高抗扰能力,或者是还有其他的更好的方式?