各位专家,请问SN74LVC8T245 和SN74LVC4245A 的有什么区别,那一款更叫适合SPI和UART_TX/RX的电平转换?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位专家,请问SN74LVC8T245 和SN74LVC4245A 的有什么区别,那一款更叫适合SPI和UART_TX/RX的电平转换?
SN74LVC4245A的电压范围为1.65 V ~5.5 V. 这样的就可以实现多个节点电压的电平转换,比如1.8V到3.3V,3.3V到5V
而SN74LVC4245A 主要实现的是3.3V到5V之间的相互转换。
如果您是需要3.3V到5V之间转换的话,二者都可以。 需要考虑能够支持的最大data rate是否满足。
另外,SPI的话,用4bit的电平转换即可,这两款都是8bit的。不用的输入端建议上拉或下拉防止悬空。