如题,区别在哪里?网站怎么没有935的资料啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
主要有三点不同:
typical sensor:913为1 MP+/30 fps
933为1 MP+/60 fps, 2 MP/30 fps
payload: 913可以为12bit/75Mhz , 10bit/100Mhz
933为12bit/100Mhz
forward line rate /backchannel rate: 913 为1.4 Gbps/2.5 Mbps.
933为1.9 Gbps/2.5 Mbps