This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教: ds90ub954 / 953 接安霸s5lm芯片 无图像



大家好,
TI员工,你们好!
按照文档配置如下:<第一位:0表示954 reg,1表示953 reg>
{0,0x4c,0x01};
{0,0x58,0x5e};
{0,0x5c,0x30};
#pll          
{1,0x06,0x49};
{1,0x07,0xF2};
#pass through 
{1,0x32,0x49};
#slave id     
{1,0x39,0x34}; //sensor i2c addr = 0x34
{1,0x41,0x34};
              
{0,0x5d,0x34};
{0,0x65,0x34};
              
#CSI_ENABLE   
{0,0x33,0x01};
              
#reset sensor 
{0,0x0f,0x7f}
三个芯片954/953/imx385 sensor  i2c读写都是正常的;
但是还是没有出图像,请问配置是否正确?
另外一种尝试方式: PGEN color bar

#Patgen Fixed Colorbar 1280x720p30
WriteI2C(0x33,0x01) # CSI0 enable
WriteI2C(0xB0,0x00) # Indirect Pattern Gen Registers
WriteI2C(0xB1,0x01) # PGEN_CTL
WriteI2C(0xB2,0x01)
WriteI2C(0xB1,0x02) # PGEN_CFG
WriteI2C(0xB2,0x33)
WriteI2C(0xB1,0x03) # PGEN_CSI_DI
WriteI2C(0xB2,0x24)
WriteI2C(0xB1,0x04) # PGEN_LINE_SIZE1
WriteI2C(0xB2,0x0F)
WriteI2C(0xB1,0x05) # PGEN_LINE_SIZE0
WriteI2C(0xB2,0x00)
WriteI2C(0xB1,0x06) # PGEN_BAR_SIZE1
WriteI2C(0xB2,0x01)
WriteI2C(0xB1,0x07) # PGEN_BAR_SIZE0
WriteI2C(0xB2,0xE0)
WriteI2C(0xB1,0x08) # PGEN_ACT_LPF1
WriteI2C(0xB2,0x02)
WriteI2C(0xB1,0x09) # PGEN_ACT_LPF0
WriteI2C(0xB2,0xD0)
WriteI2C(0xB1,0x0A) # PGEN_TOT_LPF1
WriteI2C(0xB2,0x04)
WriteI2C(0xB1,0x0B) # PGEN_TOT_LPF0
WriteI2C(0xB2,0x1A)
WriteI2C(0xB1,0x0C) # PGEN_LINE_PD1
WriteI2C(0xB2,0x0C)
WriteI2C(0xB1,0x0D) # PGEN_LINE_PD0
WriteI2C(0xB2,0x67)
WriteI2C(0xB1,0x0E) # PGEN_VBP
WriteI2C(0xB2,0x21)
WriteI2C(0xB1,0x0F) # PGEN_VFP
WriteI2C(0xB2,0x0A)

在安霸芯片端,能抓到第一个中断,但信号不完整,怀疑是 RGB888格式问题;

安霸芯片只支持RGB RAW(bayer格式),请问如何修改 PGEN的数字格式?

PGEN_CSI_DT 寄存器(default = 0x24)表示 CSI Data Type 。但bayer格式是什么值?