在电脑主机和开发板之间使用75DP159作为retimer,DP159是在开发板的输入口处,调试HDMI RX的功能。硬件设计上HPD和DDC通道没有过DP159,因此上电后主机可以检测到EDID,然后发出了有效数据和时钟(1080P输出),用示波器测试发出到DP159的in_clkx管脚的时钟频率是正确的,幅值也满足器件要求。数据通道也有数据传输。但是DP159的时钟和数据输出管脚通过示波器查看什么也没有。对于DP159的寄存器尝试三种配置方式,1、DP159默认;2、按照HDMI1.4去配置;3、按照HDMI2.0去配置;配置后依然没有输出。想询问下,DP159器件本身有那些需要配置的地方会影响到其输出。如果输入的数据不对是否会影响到时钟的输出?还有就是手头的测试板放置了有段时间,如果是器件坏了,有没有检测方法确定是DP159坏了?下面是硬件设计的原理图。