你好
请问ISO7641和ISO7141除了封装不同,功能上是否可以进行替换使用。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
隔离原理是一样的,都是电容隔离,功能是一样的,都是数字隔离器,但是需要注意的是,比如供电电压要求,最大支持的data rate,default输出状态,内部是否集成noise filter等这些电气参数的差异,如果都满足的话,那是可以替代的。